Part Number: TMDSCNCD263
Hello everyone,
I was using the AM263 CC, connected to TMDSCNHSECDOCK, without any problem. When I came back from my lunch break, suddenly, when trying to debug my project, CCS (12.2.0) returns an error:
Cortex_R5_0: GEL Output: Loading Gel Files on R5F0
Cortex_R5_0: GEL Output: Gel files loading on R5F0 Complete
CS_DAP_0: Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.10.0.00080)
I have not changed any settings from when it was working.
The same error persists with example programs from the SDK (8.5).
I tried rebooting the board, CCS and the PC. Using a different USB port doesn't help either.
The LEDs aren't indicating any error.
What can I do to solve this problem?
Thanks in advance!
Til