Other Parts Discussed in Thread: TMDSCNCD263, AM2634
We find a difference of about 10°C under the same environmental and operating conditions (same FW loaded) between the internal temperatures as read by SW via the internal temperature controller between the components mounted on our PCB (about 52°C on all 4 internal sensors) and the component mounted on its EVB TMDSCNCD263 (42°C, Tamb=20°C). our PCB and EVB have similar areas but different form factor (our PCB is rectangular with short side around 5 cm, the uC is approximately in the center of the PCB).
Checking stackup and layout regarding size and connection towards component power planes and after proper debugging of our board to exclude bus contention eventualities and other amenities that could have overloaded the Sitara, none of the above reasons seems to give an explanation.
I therefore try to ask if there could be an explanation related to internal silicon review and/or activated functionalities, because these components (being also prototipal part numbers) are from different production batches.
Specifically, looking at the marking reported above the components, they are as follows:
- EVB: XAM2634B, OLFHMZCZQ, Lot 21ACLSW G1, Prod Code 548 ZCZ
- our PCB: XAM2634B, OLFHMZCZ, Lot 23C9YQW G1, Prod Code 548 ZCZ
Looking at the component revision and feature codes the two components would appear to be the same, however as mentioned, we find the aforementioned internal temperature difference; a curious thing, is also that the 4 sensors return a very similar temperature ( 1-3 degrees difference), at least at steady state, despite 2 cores being engaged in processing and, at present, 2 being almost idle; but this could of course be due to a particularly thermally conductive intermediate layer that contributes to equalizing temperatures across the silicon...