Part Number: TMDS243EVM
I'm editing the empty.c template for a project and I'm recieving the following errors when building:
Building file: "syscfg/ti_board_config.c"
Invoking: Arm Compiler
"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -I"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/FreeRTOS-Kernel/include" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/config/am243x/r5f" -DSOC_AM243X -D_DEBUG_=1 -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_board_config.d_raw" -MT"syscfg/ti_board_config.o" -I"C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg" -o"syscfg/ti_board_config.o" "syscfg/ti_board_config.c"
subdir_rules.mk:45: recipe for target 'syscfg/ti_board_config.o' failed
In file included from syscfg/ti_board_config.c:35:
In file included from C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg/ti_board_config.h:62:
C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source\networking/enet/utils/include/enet_board.h:48:10: fatal error: 'enet.h' file not found
#include <enet.h>
^~~~~~~~
1 error generated.
gmake: *** [syscfg/ti_board_config.o] Error 1
Building file: "syscfg/ti_board_open_close.c"
Invoking: Arm Compiler
"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -I"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/FreeRTOS-Kernel/include" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/config/am243x/r5f" -DSOC_AM243X -D_DEBUG_=1 -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_board_open_close.d_raw" -MT"syscfg/ti_board_open_close.o" -I"C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg" -o"syscfg/ti_board_open_close.o" "syscfg/ti_board_open_close.c"
subdir_rules.mk:45: recipe for target 'syscfg/ti_board_open_close.o' failed
In file included from syscfg/ti_board_open_close.c:37:
In file included from C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg/ti_board_open_close.h:40:
In file included from C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg/ti_board_config.h:62:
C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source\networking/enet/utils/include/enet_board.h:48:10: fatal error: 'enet.h' file not found
#include <enet.h>
^~~~~~~~
1 error generated.
gmake: *** [syscfg/ti_board_open_close.o] Error 1
Building file: "syscfg/ti_power_clock_config.c"
Invoking: Arm Compiler
"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/bin/tiarmclang.exe" -c -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -mlittle-endian -mthumb -I"C:/ti/ccs1220/ccs/tools/compiler/ti-cgt-armllvm_2.1.2.LTS/include/c" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/FreeRTOS-Kernel/include" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F" -I"C:/ti/mcu_plus_sdk_am243x_08_05_00_24/source/kernel/freertos/config/am243x/r5f" -DSOC_AM243X -D_DEBUG_=1 -g -Wall -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function -MMD -MP -MF"syscfg/ti_power_clock_config.d_raw" -MT"syscfg/ti_power_clock_config.o" -I"C:/Users/kyle.cribbs/workspace_v12/test_am243x-evm_r5fss0-0_freertos_ti-arm-clang/Debug/syscfg" -o"syscfg/ti_power_clock_config.o" "syscfg/ti_power_clock_config.c"
Finished building: "syscfg/ti_power_clock_config.c"
It looks like the "ti_board_config.h" file included in my empty.c file can be found, the "enet_board.h" file included in the "ti_board_config.c" file can be found, but the "enet.h" file included in the "enet_board" file cannot be found. Is there something I should add to my library paths?
Thanks