Part Number: TMS570LS1224
Hi,
My need is to clock (SPI) data in from pin #105 (PGE QFP) (configured as MIBSPI1SOMI[1]) rather than from pin #94 MIBSPI1SOMI[0] .Is there any way to accomplish this?
I was thinking of using the 2-Data Line mode using MIBSPI1. Is this possible? I noticed in the Tech. Ref. Manual spnu515C 28.2.15 that 'Only module MIBSPIP5 supports Parallel Mode' . Is there any parallel mode I can use with MIBSPI1?
Thanks
Glenn