This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: Configuration Issue

Part Number: TM4C129ENCPDT

Hi,

I'm using TM4C129ENCPDT mcu to develop one of my projects on which I need to integrate TI RTOS. For that I have installed syscfg and XDCtool. By syscfg I have configured the peripherals and using XDCtool I have configured the TI RTOS. I built the project by merging both the configurations. 

1. Is this the correct way to configure the mcu for TI RTOS? or any alternative way or any other plugin available for the same?

2. In syscfg while trying to configure ethernet , only status  leds are available to configure. There are no options available in XDCtool  for the same. How can I configure Ethernet?

3. There is no option to configure the clock in the plugins. How can I configure the clock?