This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

automatic hardware memory initialization?

Hi

I want that at startup the complete RAM to be initialized with 0 zero values 

According to the TRM the register MINITGCR should be enabled = 0xA and then the corresponding bit should be written in the MSINENA register

The MSINENA is 32 bit width but which bit 0-31 should be set to enable RAM Auto initialization?

Regards

Burim