This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC software trigger usage

Hi,
About ADC module software trigger usage, according to TRM "Literature Number: SPNU489B",in section "15.3.6 How to start a conversion?", it says:


The conversion groups Group1 and Group2 are software-triggered by default. A conversion in these groups
can be started just by writing the desired channels to the respective Channel-Select Registers. For example,
in order to convert channels 0, 1, 2, and 3 in Group1 and channels 8, 9, 10, and 11 in Group2, the application
just has to write 0x0000000F to ADG1SEL and 0x00000F00 to ADG2SEL.

so, my question is:what should i do if i want to use software trigger? how to start a sample on the selected channels?