Part Number: TMS570LC4357
Hi team,
The hardware uses a 4357 development board and the code uses the HAL library's cancommunication as a reference. Use IF1 on CAN1 to control the transmit mailbox and IF2 to control the receive mailbox. The control registers are set as follows to transmit and receive extended frames:


The receive function can receive data from the chip itself when using the lookup back mode test, indicating that the hardware circuit should be fine. However, when the can pin is connected to the outside can assistant, it can only send data to the can assistant. Sending data from the can assistant makes it impossible for the code to detect data entering the cache area when the chip is received. Node->NWDATx[regIndex] & bitIndex; always is 0 and it will stuck at the point where detection data arrives making it unable to enter Getdata function.
The main function and detection data arrival are shown in the following figure:


Using the can Assistant to receive and send data is shown in the following figure:

Could you help check this case? Thanks.
Best Regards,
Cherry