Part Number: MSPM0G3507
Other Parts Discussed in Thread: UNIFLASH
Hello,
I use early samples of MSPM0G3507
From CCS I can launch debugger and my application works perfectly fine
I would like to flash, it loads correctly the ccxml file and the .out file is loaded, I selected "run target after load operation" but it seems the application doesn't start
uniflash version is 8.0.0.4026
As long as the flasher is connected, NRST pin is set low (I don' t know why), if I disconnect the flasher (XDS110) then NRST pin is set high but application doesn't run
Is there anything I shall do to release reset pin from flasher, or something to activate in CCS ?
Thanks
BR
Thomas