Part Number: MSPM0G3507
Other Parts Discussed in Thread: UNIFLASH
Hello,
I am trying to save power on an early sample
I have ADC, I2C and CAN activated
I took back the example to switch between sleep and standby mode
From current measurement I see the device doesn't switch to standby, and from the debugger it says the target reset because there is no power/clock when it tries to go to sleep or run mode
Is there something that can prevent the device from going to sleep mode?
Is it possible to use debug to test it?
Is there an example that describes how to go to sandby and go back to run? (I haven't found it but it would be ideal)
CCS 12.0 periodicaly freezes (every 5 to 10 debug attempt), it's a side comment
I also tried to call the initialisation function out of run mode but with no success
Thanks
BR
T.