Part Number: TM4C1233C3PM
Other Parts Discussed in Thread: TMS320F28069, TM4C1294NCPDT, TM4C123GH6PM, TM4C1233H6PM, TM4C129ENCPDT
Hi,
Good Day.
I bought an XDS560v2 system trace and can't flash TM4C1233 with this.
I bought the JTAG probe (XDS560v2) via the TI website and now I'm trying to flash microcontroller Tiva C TM4C1233 from CCS.
It passes the connection test but when I try to flash it CCS returns the error "Error connecting to the target: (Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If the error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK)."
I use a custom board with TM4C1233 and a stand-alone XDS560v2 System Trace. The JTAG probe is working ok, I tested it on TMS320F28069. TM4C1233 is ok too, I can program it with an ICDI programmer. The harness is ok too because it passes the connection test. They should be something in the settings.
Best Regards,
Ray Vincent