Part Number: AM2631
Hi team,
Do you have device which can support JEPG 2000 decoding? Or something like AV over IP,KVM over IP,USB over IP.
Thanks,
Zach

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zach,
Do you have device which can support JEPG 2000 decoding? Or something like AV over IP,KVM over IP,USB over IP.
It seems these items are applications, you might need to translate them to hardware/SoC requirements, map them to the microprocessors. For example, AM62x or AM62Ax provides two Ethernet ports, any Ethernet related applications can be implemented in software along with other hardware peripherals offered in the processors.