Part Number: TM4C1294NCPDT
Hi,
Memory control is verified by connecting SDRAM and QSPI-FlashROM to TM4C1294NCPDT.
Q1
When using EPI0S as an address bus and data bus, is it necessary to process a pull-up resistor, etc.?
Q2
Is it necessary to process the pins of the memory control lines assuming that they operate in SDRAM mode?
Q3
Connect to SSI of TM4C1294 for QSPI-FROM connection. Is terminal processing necessary in this case?
In either case, we are concerned about the behavior of the TM4C1294 pins when the following events occur.
(a) When power is turned on
(b) Immediately after hard reset
(c) Common to (a) and (b), after that, the software starts running and the GPIO pin assumes a predetermined role
Thanks,