Part Number: MSPM0G1106
Other Parts Discussed in Thread: MSPM0G3507,
Hi, I recently received PG2 samples of the MSPM0G3507. It is supposed to be the superset of the MSPM0G1106. Both in the 32 pins version.
I'm having an issue that I didn't have before. It is very unstable regarding to the clock. It sometimes flashes, sometimes don't. When it flashes, it mostly gets stuck in the clock verification functions, like the following ones:

Also it takes long to boot and stays here

And finally the console says this:

The configuration is set to have an XTAL of 16 MHz and run only on the external. I have programmed it as a G1106 and also as an G3507 and in either case it makes the same problem. Additional to this I have tested 4 samples and each one of them has the same problem.
We hand-soldered the microcontroller, so it may be an issue, but at least the crystal paths seem to be connected to the microcontroller (Continuity test), so it makes me think it may be a software issue.
It doesn't have this problem when using the internal oscillator. Using the SYSOSC works like charm.
Hope to see your reply soon.
Thanks
Asiel T.