Part Number: LP-AM243
I want to flash the AM243 SOC using the DFU boot-mode, from the given steps in the MCU_SDK+, we just need to point our application image file and the xip file to the default_dfu_ospi.cfg file and switch back to OSPI bootmode for the code to run.

After this change, i ran the DFU python script and it shows the SUCCESS message, but when i switch back to the OSPI bootmode, the PC fails to detect the device as a USB device.

Are there some more steps required to correctly flash using DFU?