Hello,
we are currently writing our own flash-driver and I got into the OSPI-part in the TRM. I noticed the OSPI also supports automatic polling of the WIP-register of the Flash via the OSPI_WRITE_COMPLETION_CTRL_REG. But I also noticed the sdk-flash-driver does that in SW. Also I found some comments inside the OSPI-driver in the open-function stating that "Set an invalid opcode in the WRITE_COMPLETION_CTRL_REG due to IP limitation".
Which I guess could mean it's not functional?
I didn't find any hint on this in the errata of the AM243x.
Are there more known limitations the OSPI has compared to the functionality stated inside the TRM?
Best regards
Felix