Part Number: UNIFLASH
Hello Community,
I installed "uniflash_sl.8.3.0.4307.exe"
The destination folder I installed it to was "C:\Program Files(Misc)\ti\uniflash_8.3.0".
I do not have any hardware or peripherals connected to the computer. I immediately get the error when trying to launch the program.
Can someone please help me with the following error?
"Error Loading Extension" "Failed to load extension from: C:\Program. Manifest file is missing or unreadable."
Thank you!