Part Number: AM2434
Our customer wants to connect multiple devices to OSPI.
I understand that it is not recommended that multiple devices are connected as discussed in other threads.
e2e.ti.com/.../am6442-is-it-possible-to-connect-4-devices-to-ospi-using-4-css
On the other hand, I understand that it is possible to connect multiple devices if OSPI is used at 50 MHz or even lower speeds.
But I cannot find out how to configure for each chip select in the TRM.
Can each chip select be configured differently?
Best regards,
Daisuke