This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello again,
I am working on a small PCB to test some functions of the MSP432E3401Y. I have a few questions if anybody has a spare moment:
Thank you for any help you can give me,
Dan
- Pins 66 (XOSC0) and 67 (XOSC1) are only used as a clock during hibernation, correct?
Yes
- If so, can XOSC0 be drawn to ground, and XOSC1 left NC as shown in Table 4-6 if not using the hibernation feature?
Yes,
- Are pins 88 and 89 (OSC0 and OSC1 respectively) meant to connect to a driving crystal oscillator?
Yes
- If OSC0 is drawn to GND, and OSC1 is left NC, is the device driven by an internal clock?
Yes, by internal PIOSC
- Will not having either of these external oscillators interfere with JTAG or ADC functions?
As long as internal PIOSC is running as a source for system clock, you will not have problem with JTAG or ADC.