Part Number: TMS570LC4357-EP
Other Parts Discussed in Thread: TMS570LC4357
Hi Team,
My customer wants to use the EMIF communication method to allow TMS570LC4357 to communicate with the FPGA. The MCU application program is placed on the off-chip SDRAM mounted on the FPGA. After the MCU is powered on, it directly runs the application program in the SDRAM (FPGA). How should it be done?
My customer checked the information, and he thinks that the CMD file can be modified to define the starting address of the application. Is this address the address of SDRAM?
After he enables the EMIF bus in the bootloader, what else needs to be done?
MEMORY
[
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0007FFE0
FLASH1 (RX) : origin=0x00080000 length=0x00080000
FLASH2 (RX) : origin=0x00100000 length=0x00080000
FLASH3 (RX) : origin=0x00180000 length=0x00080000
EXTFLASH (RX) : origin=0x60000000 length=0x00080000 // Is this starting address the address of the SDRAM mounted on the FPGA?
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x00026B00
]
--
Thanks & Regards
Yale