Part Number: TMS570LC4357
Hi all:
I use F021 API to erase bank1 and bank7 then it cause ESM error which is ECC broken. I have some questions about ECC.
1. In the trm page 121, Memory map. I find 0xF000000 to 0xF047FFFF is a place to store flash ecc , opt and eeprom. So Are there all flash ecc stored in this place but not in bank0 or bank7?
2. If I earse bank1 and bank7 by using " Fapi_issueAsyncCommandWithAddress(Fapi_EraseBank, (uint32_t*) 0xF0200000u);" function, will it case ECC error? After earsing any flash banks in my project, Do I need fill ECC by myself?
3. How ecc error occur? For example, if I just read flash, will cpu do ecc caculating?