Part Number: TMS570LC4357
Hi team,
Regarding the device manual spnu563a, the customer has some questions:
1) As per the manual, angle increment = new angle cnt - old angle cnt:

While the HET Interface is an 11-bit counter that continuously accumulates the angle increment. What does this 11-bit counter do? Which module uses this counter value?
Also, based on the figure below, why would the 4-bit angle increment data come from this counter?

2)

Regarding the above figure, dose it mean that if the current angle increment = 31, the HWAG will pass the angle increment to the HET three times, with a value of 15, 15, and 1. If so, what is the timing?
3) How is the angle tick generated?
The count period of SCNT is P(n-1)/K, and SCNT generates an angle tick each time P(n-1)/K is counted, up to K angle ticks in one gear signal period.

However, the document also states that SCNT counts in K steps until P(n-1) is exceeded to produce an angle tick.

Could you help check these 3 questions? Thanks.
Best Regards,
Cherry