Part Number: MSPM0L1306
Hi,
I have some questions about pin mapping for the MSPM0L1304xRHBR. (32 VQFN package)
1. PA18 (BSL invoke Pin)
PA18 pin is BSL invoke pin. However it is also used for other functions as following.

Is it possible to use it as an analog pin?
PA18 requires a pull-down resistor to prevent BSL entry.
When PA18 is used as an analog pin like ADC, OPA1_IN0+ or GPAMP_INUART0, doesn't the pull-down resistor affect the input?
2. JTAG ports
PA20/SWCLK/A6 pins cannot be used as GPIO or A6 during debugging?
3. GPIO interrupt pin
GPIO interrupts seem to be possible on all pins.
But GPIOs for wakeup from shutdown mode seem to be part of it.

If it is right, there are only 4 GPIOs (PA0, PA1, PA17 and PA18) for wake up function on 32 pin device.
Is my supposition correct?
Thanks.