Part Number: AM2634-Q1
What wil be the maximum current drawn by the VDD during the normal operation of controller? In page no 67 of datasheet, The Maximum Current Rating for Core Domain (VDD+VDDARn) is given as the 2.5A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The maximum current rating for VDD + VDDAR is 2.5A.
Also as the power consumption is highly dependent on use case, please use PET https://www.ti.com/lit/an/sprad54/sprad54.pdf to model and see the VDD/VDDAR power for a given use case.
For typical use case power consumption you can refer to 7.7.2 Power Consumption - Typical and 7.7.3 Power Consumption - Traction Inverter.
Best Regards, Shiv