Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Hello everyone,
I am having some issues with the UART0 module of the MSPM0L1306.
If I map the UART0 RX pin to PA9 everything works fine. An interrupt is thrown as configured once data is received. But if I reconfigure the UART0_RX pin to be on PA18 nothing is being received anymore. Transmit is still working fine. All registers from the UART are configured exactly the same, the only difference is that the IO MUX 19 is now set to the alternative function 2 (UART0_RX).
Has anyone else experienced the same issue?
PA18 does not work
PA9 works fine