Other Parts Discussed in Thread: DP83849IF, , TM4C1292NCPDT, TM4C129DNCPDT
I'm hoping that there is a design guideline or that someone here has experience with adapting, for example, the evaluation kit design from the RJ45 connector and magnetics to an SFP connector/module. It seems like it should be as simple as taking the differential Tx and Rx from the SFP to the micro just like with the RJ45 but I have not found any information in the SFP documentation or in Tiva docs about the necessity of the magnetics and what, if any, terminations are needed. Also, I believe that the SFP will require at least the Rx LOS signal into the ethernet PHY but I would guess i would need to change some setting in the registers for the phy to point to whatever GPIO is used for that signal. Anyone able to help, thanks!