Part Number: MSPM0G1106
Hi team,
From the datasheet, the maximum value of VIL is 0.3*VDD. How is it measured?
Best regards,
Shunsuke Yamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G1106
Hi team,
From the datasheet, the maximum value of VIL is 0.3*VDD. How is it measured?
Best regards,
Shunsuke Yamamoto
Hi Shunsuke,
Maximum value of VIL means that the max input voltage which will be recognized as a low voltage level. If it exceeds the max VIL, and meanwhile it is lower than min VIH, then the input IO data is uncertain, it may be high or low, which is not recommended.
B.R.
Sal