This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: latest SDK problem

Part Number: MSPM0G3507

Hi Team,

There's an issue from the customer need your help:

Use the latest SDK development kit ( mspm0_sdk_1_00_01_03 ) to program the erasing FLASH processing, the test found that only the first 32K can be erased, and the latter cannot be erased; and the previous version of the SDK ( mspm0_sdk_1_00_00_04 ) does not have this problem (Note: the same The flash operation function written by myself calls different SDK underlying drivers); is it a problem with the latest SDK package or requires special handling?

Could you help check this case?

Thanks & Regards,

Ben

  • Hi Ben,

    It is a known issue about the Flash operation with the SDK (mspm0_sdk_1_00_01_03).

    And we have fixed this issue in the next version SDK, which is planned to be released in ti.com about a week later (in early July).

    If the customer is urgent and please email to me, and I can give your a file to fix it temporarily.

    B.R.

    Sal