Part Number: LP-AM243
Hi,
I’m using AM243x Launch pad, I need to configure Timer. As per image it is showing that only way to implement timer is DM Timer implementation.
Whether this timer can be configured as RTI up counter/ free running counter ? (Because I can able to see that in am243x TRM document that RTI8 is dedicatedly used for R5FSS0_CORE0).
And also what is the use case of TimerP_rti.c file (path : mcu_plus_sdk_am243x_08_05_00_24\source\kernel\nortos\dpl\common\ TimerP_rti.c) ? (same Timer APIs are used in this file but implementation is changed).


Kindly give clarification/ suggestion on the above query.
Thanks in advance