This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: Can I configure am243x Launchpad timer as RTI up counter\free running counter

Part Number: LP-AM243


Hi,

I’m using AM243x Launch pad, I need to configure Timer. As per image it is showing that only way to implement timer is DM Timer implementation.

Whether this timer can be configured as RTI up counter/ free running counter ? (Because I can able to see that in am243x TRM document that RTI8 is dedicatedly used for R5FSS0_CORE0).

And also what is the use case of TimerP_rti.c file (path : mcu_plus_sdk_am243x_08_05_00_24\source\kernel\nortos\dpl\common\ TimerP_rti.c) ? (same Timer APIs are used in this file but implementation is changed).

Kindly give clarification/ suggestion on the above query.

Thanks in advance