Part Number: AM263P4
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello.
I have several questions about RTI counter configuration
1. Is there any possibility to set compare value of the up counter to maximum 0xFFFFFFFF value with SysConfig? It allows input only of integers value to 'Desired Output Frequency (Hz)', and 1 Hz is actually minimal value available. Entering '0' seems give required behavior, but also leads to 'division to zero' warning.
2. What is 'NTU' signal? I found this in SDK API and register addendum, but no any description in reference manual.
3. What affect parameter 'clkSrc' in 'RTI_counterConfigure' function? I found this picture in reference manual, but no any descriptions in text about FRC clock select. Which values are valid?