Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I have project which was written for core 0-0 with all the peripherals defined (IO, ADC, PWM, CAN etc.). I've tested the project on core 0-0 as a single core and it works fine. Now I have another core 0-0 project with only CAN on it which also works individually. Now I'm trying to move the 1st project with all the peripherals except CAN to core 1-0 and trying to work the CAN project on core 0-0 to make it a multi-core project with IPC communicating between them.
Now I have;
Core 0-0 running project with only CAN and IPC
Core 1-0 running project with all peripherals & IPC except CAN
What I noticed was that I have blinky on both projects and it works I have even confirmed that the IPC is working but the CAN comms is not working.
My question is can you please provide any document that would list steps needed for moving the core 0-0 project to core 1-0 if not can you please list all the necessary changes that needs to be done when moving the cores.
Regards,
Harsha