Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1305: can not debug by Keil5

Part Number: MSPM0L1305
Other Parts Discussed in Thread: SYSCONFIG

Hi Team,

I ask this question for our customer:

my custom board mcu is MSPM0L1305, and i use SKD (mspm0_sdk_1_00_00_04) sample to create my keil project. now can download the project into flash, but can not run, the keil log as following:

Set JLink Project File to "C:\ti\L42P-APP\keil\JLinkSettings.ini"* JLink Info: Device "MSPM0L1305" selected.
 
JLink info:
------------
DLL: V7.82 , compiled Oct 13 2022 13:32:51
Firmware: J-Link V9 compiled May  7 2021 16:26:12
Hardware: V9.30
S/N : 59300616 
Feature(s) : RDI, FlashBP, FlashDL, JFlash, GDB 
 
* JLink Info: Found SW-DP with ID 0x6BA02477
* JLink Info: DPIDR: 0x6BA02477
* JLink Info: CoreSight SoC-400 or earlier
* JLink Info: Scanning AP map to find all available APs
* JLink Info: AP[5]: Stopped AP scan as end of AP map has been reached
* JLink Info: AP[0]: AHB-AP (IDR: 0x84770001)
* JLink Info: AP[1]: MEM-AP (IDR: 0x002E0001)
* JLink Info: AP[2]: JTAG-AP (IDR: 0x002E0000)
* JLink Info: AP[3]: MEM-AP (IDR: 0x002E0003)
* JLink Info: AP[4]: MEM-AP (IDR: 0x002E0002)
* JLink Info: Iterating through AP map to find AHB-AP to use
* JLink Info: AP[0]: Core found
* JLink Info: AP[0]: AHB-AP ROM base: 0xF0000000
* JLink Info: CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
* JLink Info: Found Cortex-M0 r0p1, Little endian.
* JLink Info: FPUnit: 4 code (BP) slots and 0 literal slots
* JLink Info: CoreSight components:
* JLink Info: ROMTbl[0] @ F0000000
* JLink Info: [0][0]: E00FF000 CID B105100D PID 000BB4C0 ROM Table
* JLink Info: ROMTbl[1] @ E00FF000
* JLink Info: [1][0]: E000E000 CID B105E00D PID 000BB008 SCS
* JLink Info: [1][1]: E0001000 CID B105E00D PID 000BB00A DWT
* JLink Info: [1][2]: E0002000 CID B105E00D PID 000BB00B FPB
ROMTableAddr = 0xF0000000
* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.
* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.
 
Target info:
------------
Device: MSPM0L1305
VTarget = 3.309V
State of Pins: TCK: 0, TDI: 0, TDO: 0, TMS: 1, TRES: 1, TRST: 0
Hardware-Breakpoints: 4
Software-Breakpoints: 8192
Watchpoints:          2
JTAG speed: 4000 kHz
 
Load "C:\\ti\\L42P-APP\\keil\\Objects\\L42P_APP_FW.axf" 
* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.
* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.
*** error 122: AGDI: memory read failed (0x01000020)
* JLink Info: CPU could not be halted
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 16 (XPSR) while CPU is running
***JLink Error: Cannot read register 0 (R0) while CPU is running
***JLink Error: Cannot read register 1 (R1) while CPU is running
***JLink Error: Cannot read register 2 (R2) while CPU is running
***JLink Error: Cannot read register 3 (R3) while CPU is running
***JLink Error: Cannot read register 4 (R4) while CPU is running
***JLink Error: Cannot read register 5 (R5) while CPU is running
***JLink Error: Cannot read register 6 (R6) while CPU is running
***JLink Error: Cannot read register 7 (R7) while CPU is running
***JLink Error: Cannot read register 8 (R8) while CPU is running
***JLink Error: Cannot read register 9 (R9) while CPU is running
***JLink Error: Cannot read register 10 (R10) while CPU is running
***JLink Error: Cannot read register 11 (R11) while CPU is running
***JLink Error: Cannot read register 12 (R12) while CPU is running
***JLink Error: Cannot read register 13 (R13) while CPU is running
***JLink Error: Cannot read register 14 (R14) while CPU is running
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 16 (XPSR) while CPU is running
***JLink Error: Cannot read register 17 (MSP) while CPU is running
***JLink Error: Cannot read register 18 (PSP) while CPU is running
***JLink Error: Cannot read register 20 (CFBP) while CPU is running


and keil project options as following:

--

Thanks & Regards

Yale

  • Hi Yale,

    How dose customer connect the PA18? Dose they use it as BSL trigger function? If not have they modify the non-main flash?

  • Hi Gary,

    Thanks for your reply.

    Your judgement is correct. The customer multiplexed the PA18 pin for AD. They connected this pin to Battery, so it is pulled up, MCU run into BSL mode.

    They have further question:

    1. How can PA18 be multiplexed as the AD function of detecting high level voltage?

    2. According to TI's documentation, the BSL_invoke function of PA18 can be disabled, that is, it can be configured as disabled using sysconfig. But it doesn't work with Keil IDE. Keil IDE does not write BSL_CONFIG and BCR_CONFIG into the non-main area of flash. Refer to the "flashctl_nonmain_memory_write" routine, write the BSL_CONFIG and BCR_CONFIG configuration parameters to the non-main area through the program, and there is no chance to run the program to write these two configurations to disable the GPIO BSL_Invoke function when PA18 is pulled high. In this case, whether the software can Disable GPIO BSL_Invoke function?

    3. The customer uses the "flashctl_nonmain_memory_write" routine to write the non-main area of the flash to disable the GPIO BSL invoke function, and the Flash is locked. How to unlock it?

    --

    Thanks & Regards

    Yale

  • 1. How can PA18 be multiplexed as the AD function of detecting high level voltage

    They can modify the non-main flash for the steps you can refer to this document section 5.3

    https://www.ti.com/lit/an/slaaec9/slaaec9.pdf