Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507, SYSCONFIG
Hello,
I want a falling edge on an input capture to trigger a DMA unit.
The MSPM0G3507 is in sleep mode. When a falling edge is detected, I want the trigger to fire and the timer value to be written from the register to an array via DMA. The MSPM0G3507 shall leave the sleep mode only when the distance between two falling edges is greater than 100us.
How can I achieve that an input capture triggers a DMA unit on falling edges?