Part Number: TMDSEMU200-U
Other Parts Discussed in Thread: UNIFLASH
Hello I am trying to run a cmd for uniflash to load a bin file, but every time I run my command I get that I am unable to open the file
This is the command example
dslite --mode load --config=file.ccxml [options] coff-or-binary-file1
Options:
-c [ --config ] arg Configuration (ccxml) file.
-f [ --file ] arg Elf, coff or binary file(s) to flash or verify. To
specify a binary file, append ',address' after the
file. This option exists only for compatibility - the
file to load can instead just be passed as the last
token on the command line.
-t [ --timeout ] arg Timeout in seconds, infinite if unspecified.
-g [ --log ] arg Enable detailed logging to the specified file.
-r [ --core ] arg (=0) Zero based index of core to operate on.
-h [ --help ] Print this message.
And this is my command in cmd
C:\ti\ccs1230\ccs\ccs_base\DebugServer\bin>dslite load -c C:\Users\julioam\ti\CCSTargetConfigurations\Mutiflashing2.ccxml -f -binary-'C:\Users\julioam\ti\CCSTargetConfigurations\M1158001.V34909.bin'
DSLite version 12.3.0.3006
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
GEL: CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
Connecting...
Failed: Unable to open file: -binary-'C:\Users\julioam\ti\CCSTargetConfigurations\M1158001.V34909.bin'