Part Number: LAUNCHXL2-TMS57012
Other Parts Discussed in Thread: TMS570LS1224
Hello team,
My case is: I have a LAUNCHXL2-TMS57012 and I'm designing a prototype where I use the same MCU as the launchpad (TMS570LS1224).
My idea is to use the launchpad to debug the MCU in my prototype. I would connect my computer to the launchpad via USB, and the launchpad to my PCB through J1 connector, following the steps:
- Place J1 connector on the launchpad
- Supply the launchpad with 5V and GND coming from my PCB
- On my PCB, place a connector to receive the launchpad's J1 signals
- Route these signals to my PCB's MCU, in the same way as it is in the launchpad
From what I see, I would upload the CCS project to both MCUs. But, as I will not use the one at the launchpad, I does not matter. I think whthat I might have a problem while running the program while the boards are connected, but after I separate them, it should work normally, would it?
Is this going to work? Is there any other precaution that I need to have in this process?
Thanks in advance,
Guilherme Pissaia