Other Parts Discussed in Thread: SYSCONFIG
The TRM for the MSPM0G3507 lists FRANGE=7 for bus clock 40-48MHz

However, my ADC code seems to work with a bus clock of 80MHz. The data sheet also lists the ADC0/ADC1 as both PD1 and PD0.
1) Is the ADC in PD0 so the CPU clock of 80 MHz is actually 40MHz at the ADC?
2) Is the ADC in PD1, so the CPU clock of 80 MHz is actually 80MHz at the ADC, but FRANGE=7 is correct?
thanks