Part Number: TM4C1294NCPDT
Hi, I'm using DMA with UART RX on the TM4C1294NCPDT at a baud rate of 230400. The chunks of key/value delimited data I receive is of variable size and in no predictable order. Sometimes the key/value pair I receive is as short as just a few bytes and other times it's as long as 50 to 60 bytes.
I'm using DMA in ping-pong mode where the primary and alternate buffers are each 64 bytes. However, I need to process the key/value data as quickly as possible, preferably, as soon as I get each key/value pair I would like to process it. Of course, if I happen to receive a series of key/value pairs where each is only a few bytes long, it will take many key/value pairs before the 64 byte DMA buffer is full, substantially delaying how quickly I can process the earlier key/value pairs.
I was hoping there is some way to "peek" into the current DMA buffer being populated before it is entirely populated and process any existing key/value pairs available, however, after reviewing chapter 9 of the "Tiva TM4C1294NCPDT Microcontroller" data sheet in great detail, I'm not seeing a way to reliably "peek" into the DMA buffer before it's complete.
What I really need to know is where the current DMA write pointer is pointing to for the next RX byte received, but I'm not seeing that this is available.
Is this in fact not available or am I missing something?