Part Number: TMS570LC4357
Other Parts Discussed in Thread: UNIFLASH,
Hi all:
I have a qs on ECC generation. The memory map of LC4357 in page 121 in trm which shows me the location of "Flash ECC". The more specific address is from 0xF040_0000 to 0xF05F_FFFF.
I have three questions about this address:
1. When I use UNIFLASH to download the new hex file into LC4357, and I choose the "Auto ECC generation" and "Entire Flash", will the uniflash erase this address( 0xF040_0000 to 0xF05F_FFFF.)?
2. When I use F021 lib to erase and write flash, will the f021 lib will generate the ecc automatically?
3. When I use UNIFLASH erasing the whole flash, I think the data in flash should be 0xFFFF_FFFF,. However, when I reading through uniflash, I find the values of flash are not 0xFFFF_FFFF, maybe 0xFF3E_FFEF or something else, why?
Thanks & Regards
Li