Other Parts Discussed in Thread: EK-TM4C1294XL
Hi, we are working on a releasing a new product using the TM4C1294NCPDTI3.
I am trying to test out the bootloader function using LM Flash Programmer on my computer, but I am not able to. It works fine on my colleague's computers, but we can not get it to work on mine. I am using the same settings and the same equipment. I would like to find a solution as if it is a problem for me, it also has the potential to be a problem for our customers.
I have it set to manual configuration and am using Serial (UART) interface.
I've confirmed that I am using the right com port. I can communicate with the device using other programs (which are no longer connected and not blocking the port). If I change the com port to one I know is wrong on LM flash programmer, then I get an error saying that it has failed to configure the com port. I am not getting that error when I have it on the right com port, so I know that it is able to use that com port.
I know the correct baud rate (again - able to communicate through other programs). However, I am using the 'Auto Baud Support' feature. When I try to connect, i get an error saying that it 'failed to synchronize the baud rate with the board'. When I disable the auto baud support, then the error says 'failed to establish communication with the board'.
I started by using a USB hub, but I saw in LMFlash Help that it can mess things up, so now I am connected directly to a usb port on the computer and not through a hub. From the USB port, I have a USB-RS485 converter. I have tried different brands of converters to see if it was a problem there. It does not seem to make a difference.
I've also tried completely restarting my computer.
These are the same settings my colleagues are using successfully. I am in bootloader mode on the device when attempting to connect. Could you help me troubleshoot why I am having a problem?
Could it be something to do with the drivers on my computer? I have different FTDI drivers for the converters.
Could a security setting be messing with LM Flash Programmer's ability to communicate?