This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS570LS31HDK: Confirming Flash information.

Part Number: TMDS570LS31HDK

Hi there,

I've read through the TMS570 TRM, Safety Manual, and Datasheet, but I wanted to confirm some facts about the Flash. Please correct me if I'm wrong:

  • There are 3 Flash banks: 0, 1 & 7.
    • Banks 0 & 1 are considered TCM connected to the CPU.
    • Bank 7 is external and is used for Flash EEPROM emulation.
    • All 3 banks contain two extra sectors, a customer OTP and a TI OTP.
  • Only TCM banks 0 & 1 are accessed on Bus 1.
  • Bank 7, and all OTP memory are accessed on Bus 2, despite some of the OTP physically being located in banks 0 and 1.
  • Syndrome calculation is only applicable to Bus 2 (OTP & FEE) as Diag Mode 2/3/4 test the syndrome and only work on Bus 2

Namely on the Syndrome calculation, I'm not sure if it is done on Bus 1 as well (TCM Flash). Can someone please clarify this for me? Thank you!