Part Number: AM2632
Other Parts Discussed in Thread: LP-AM263
Hello,
we are using AM263x (Launchpad) at the moment, but in our final layout, we will use AM2632.
We have a question for the PRU-Unit of the AM263x. Is it possible to access other GPIOs form the PRU, than the mapped GPIOs of R30/R31?
How can we configure the GPIOs, to be operated from the PRU?
What did we up to now?
We set up a small example firmware for the PRU0, this is loaded and startet from the R5F at run up. The small firmware of the PRU increments only a variable at the moment, which we can read from the R5F controller (from the memory).
Our idea is, to handle a large amount of inputs/outputs by the PRU (more than the 20 register-mapped IOs). The R5F should write the output-values to memory and read input-values from memory only.
How can we configure such a system (especially thew GPIO-mapping).
Thanks for your answers.
Best regards
Jo Scho