Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: UNIFLASH,
Follwed the below steps to enable the TI boards before usage.
Using xdsdfu commands in cmd window
1. Switch to DFU mode
2. Program firmware_3.0.0.19.bin
Post that launch Uniflash application
1. Device is detected.
2. Select the file aevm_1_0_3_5.txt
3. Click on load image
Once the device is successfully programmed, the USB cable is removed and plugged to U7 port of MSP board, the device will get detected automatically.
Note:
1. The above procedure was used for programming the other TI MSP-EXP432 boards - Successfully.
2. Used xdsdfu commands & Uniflash tools only
However, during the above process, 4 boards are having the below-mentioned issues.
Issues:
1. On 2 TI MSP boards, Unable to program the MSP-EXP432E401Y with flash bin "aevm_1_0_3_5.txt" using the Uniflash tool.
Error:

2. On another 2 MSP TI432E401Y boards, Able to program the MSP-EXP432E401Y with flash bin "aevm_1_0_3_5.txt" using the Uniflash tool. Once device is programmed the USB Cable is removed and connected to U7 usb port. The device is not getting detected in device manager [i.e ACCtrl ports are not detected]