Part Number: RM57L843
Hi TI Team,
I have worked on a Ethernet Bootloader as supported by you from below link,
I got Ethernet bootloader is worked well. I got the image file was transferred into the microcontroller.But same of my application code is not executing.The application image was transmitted successfully but that not executing.I have attached the project above.What are the changes i have to made.
And the other question is the same Ethernet cable can be used for transfering data and can be act as bootloader. Is it possible.What are the way to do that.
Thank in Advance
Best Regards,
A.Ajith Kumar