Part Number: TM4C123GH6PM
Hello
I have a TM4C123GH6PM works fine for few time and then stop and not working again until i leave it un-powered for few days, What would be the issue here?
BR
Hani
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123GH6PM
Hello
I have a TM4C123GH6PM works fine for few time and then stop and not working again until i leave it un-powered for few days, What would be the issue here?
BR
Hani
Hi,
Can you elaborate what is not working? Is it that you cannot connect to the device using the debugger? Or is it that you cannot download new firmware? Or the application firmware does not run after loaded. Please be specific.
Personally, I have not heard of a forum reporting that a device first works for a few times and then stop working and finally after waiting for a few more days the device works again. The only thing I can think of is temperature related but you will need to do some experiments to isolate the problem. This is what I will suggest you do.:
- Does it fail more quickly if you raise the operating environment temperature? You will need to heat up the board using a heat gun or use some type of ThermalStream equipment to raise the DUT temperature.
- Does it fail less quickly or stop failing if you reduce the operating environment temperature? You will need to cool down the device using some type of ThermalStream equipment.
- Do a ABA swap test.
The A-B-A Swap Method is a simple cross check test, which can confirm the observed issue is not systemic.
Step 3 is important because it helps us to exclude any possibility that the issue is caused by a systemic issue or the interaction of multiple slightly bad components on a good board.
Once you have the results and if you prove 100% it is a MCU problem then you can contact the local TI office for quality return process.
Thank you Charlos, but we discovered the issue was due to hidden extra flux under the MCU whiche caused the issue
BR
Hani