Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: AM2634
Hello,
Regarding the example: ipc_notify_echo_am263x-cc_system_freertos_nortos
<Questions>
1) Even though this example is specifically for the Control Card (cc), the system project Target Configuration General Set-up does not select the _CC device. Why is this please?

2) In the Target Configuration Advanced set-up, only R5_0 is associated with an initialization script (GEL) file. Why isn't the script required for the other cores?

3) The Prerequisites instructions for this example tells us to modify the AM263x.gel file to be able to use all four cores (2 x dual core) as independent cores:
C:/ti/mcu_plus_sdk_am263x_08_05_00_24/docs/api_guide_am263x/CCS_LAUNCH_PAGE.html#PREREQUISITES
In the scenario where I want dual core for R5_0/1 but keep lock-step for R5_2/3, do I need to make multiple gel files: a) mode = 1 and b) mode = 0 and assign a) and b) to R5_0 and R5_2 respectively?
Thank you.