Part Number: MSPM0L1304
Hello,
We started with the qualification of a custom board with the MSPM0L1304 CPU on it. The following is applicable:
-Power supplies are ok
-I connected the XDS110 pod using SWD
-Signal integrity is ok
The steps I made:
-I am able to setup a project based on a default CCS program
-I created a target configuration
-I was able to verify the connection -->"The SWD Mode Integrity test has succeeded."
But I cannot load the program:

-After this a CPU power cycle is required.
Is there an example project available? I think some files are missing? I also tried to check the SWD password. But so far no access. The development kit with 1306 CPU is working fine.
Could you explain what might go wrong?
Thank you in advance!