This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: First Connection Problem in Serial Port Connection

Part Number: TMS570LS3137

When I connect to the processor through the serial port, I cannot send or receive any commands unless I do a hardware reset to the processor. 

When the processor is connected, when I press the reset button on it, I can receive and transmit data.

Is there a function or code that can perform an automatic software reset when I connect to the port?

There may be another alternative solution.




Thanks & regards.