Part Number: RM48L540
Hi,
Could I used XDS110 programmer debuger for RM4X series microntroller?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rohit,
Could I used XDS110 programmer debuger for RM4X series microntroller?
Yes, you can use XDS110 programmer debugger for RM4X series microcontroller.
XDS100V1/2/3, XDS110, XDS2xx, and XDS560x can be used for Hercules devices in TI CCS.
--
Thanks & regards,
Jagadish.

Hi Jagadish,
Please checked schematic of MCU and debugger connection with watchdog along with 3.3Volt, 1.2Volt and 2.5Volt supervisory section. Please let me know is that workable or not.
Hi Rohit,
Please make sure the connections are as per below circuit:

This is from RM46 launchpad and complete schematic can be found in the below link:
LAUNCHXL2-RM46 Development kit | TI.com
There won't be any difference in JTAG circuit wise between these two devices. So you can refer above JTAG connectivity and use same connectivity.
--
Thanks & regards,
Jagadish.