Part Number: TMS320C6655
I am redoing Nor Writer with modifications
Trying to use another flash memory
It seems to do memory write
The following error message is displayed in the console
--------------------------------------------------------------------------
[C66xx_0] NOR Writer Utility Version 01.00.00.03
Flashing sector 0 (0 bytes of 136164)
Flashing sector 1 (65536 bytes of 136164)
Flashing sector 2 (131072 bytes of 136164)
Reading and verifying sector 0 (0 bytes of 136164)
Failure in sector 0, at byte 0, (at byte 0 in the data file) expected 0x000000ff, read 0x00000040
NOR read verify failed
----------------------------------------------
I need an answer.
thank you